Button
Triggering an action
A button that is not a submit button is styled differently to indicate it performs a secondary action, either launching a dialog, triggering an action on the page or something custom to the workflow
A button that is not a submit button is styled differently to indicate its unique function. It performs a secondary action, which most of the time includes launching a dialog to populate data on a table. However, each workflow can add buttons to perform custom actions based on their needs.