Select

Creating predefined answers

A select list presents a list of choices. Only the listed values can be used as valid data. Choices come in two distinct field types:

A Select List is a field that exclusively allows predefined answers provided when you activate the list. To activate the list, click on the text field, and you'll see a list of acceptable values. You can scroll through the list or, for a more efficient approach, begin typing to filter the list and find your desired value more quickly. To select your value, press the down arrow key, and then hit enter.

Note: Tab Key: Using the tab key will not shift your cursor from the select list input to the drop-down list. By default, the tab key will move to the next field in the form. To cycle through the select values, use the up and down arrow keys.

Example

The default style
  • Text Item Custom description

Has a default initial value
    You cannot interact with this element
      This has an error you need to resolve