Text Content
Displaying read only data
Overview
Barcode
The text-content field is a read-only area for text. Since it is read-only, use it for informational, symbolic or warnings.
Features
- Static Content: You can add static content for informational or warning purposes. The most common use for textcontent is text within a select lists.
- Dynamic Content: You can link a textcontent field to a database field so it populates when from your form's data.
Example
Some short or really long text can go here Some short or really long text can go here
- Opt-in Formatting: By default, the text on the page will be formatted based on
its positioning, However, the format, such as new lines and spacing, can be
preserved as it is typed in the database by adding the
preserve-formattingformatter.
Opt-in Formatting
Text on this first line Some on the second. Text on this first line Some on the second.